AXIS#.IL.PWMQUIET

Description

0 - Operate at nominal PWM modulation frequency only. The nominal frequency limits power consumption, but results in acoustic noise.

1 - Automatic control of PWM modulation frequency. Operate at maximum frequency, outside the audible range, when allowable, to eliminate acoustic noise.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

N/A

Range

0 to 1

Default Value

1

Data Type

Integer

See Also

AXIS#.IL.KP

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.IL.PWMQUIET

500ah

17h

Unsigned8

-

-

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

5828

1

5828 (0x16c4)

AXIS1.IL.PWMQUIET

Unsigned8

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS1.IL.PWMQUIET

5828

Unsigned8

Read/Write

-

Related Topics

"Current Loop"